Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Do we offer a filler module for use in empty slots of the M340 backplane?

No, we don't offer a filler module but we do offer a cover which can be placed over the backplane connector. Its part number is BMXXEM010 and there are 5 covers included in the package.




R-82117