Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the replacement of the XBTG6330?
The XBTGT6330 was the replacement for the XBTG6330 but it is now obsolete.

The XBTGT6330 has been replaced with the HMIGTO6310 or the HMIG3U + HMIDT642 screen

Both targets have the same cutout dimension.  See attachment for specification

Vijeo Designer V6.2 SP6 is required.  If the current application is older than V5.0 it will need to be updated.

You can contact Schneider Electric tech support for the update.

Schneider Electric Saudi Arabia

Attachment(s)
Transition Tool for XBTGT6330.pdf [826.96 KB]