Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why am I getting an error message: "PLC return error code FDH-83,80H" when communicating between a Magelis and a Unity Quantum PLC?

Issue:
Getting an error message: "PLC return error code FDH-83,80H" when communicating between a Magelis and a Unity Quantum PLC


Product Line:
Vijeo Designer, Quantum PLC


Resolution:
The error message is due to the Magelis reading the discrete/analog inputs as %I or %IW from the Unity Quantum. You will need to delete the tags and link to the Unity database file. Then re-link the tags back into Vijeo Designer and check the box to "force IO to unlocated variables". Or convert all of the input variables to memory bits and words.