Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do I compare two Somachine projects?

Goals and Symptoms

This Resolution is to show customer how to add the compare feature of Somachine and then compare two projects.

Causes and Fixes

First, you need to enable the compare feature in Somachine. By going into Tools Menu -> Customize (see screenshot below).
image1

From the bottom left window select "File" and on the bottom right window select "Compare". Then select the Add Item button (see screenshot below).
image2

Now you will see the compare in the top window (See screenshot below).
image3

To compare, you need to go to File Menu -> compare (See screenshot below).
iamge4

From the compare window you either need to select a local file or from a control database (See screenshot below).
image5