Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does the PID blocks in Unity Pro/EcoStruxure Control Expert have a setting for ON - OFF control?

Issue:
On-OFF control for PID function block in Unity Pro/EcoStruxure Control Expert


Product Line:
Unity Pro, EcoStruxure Control Expert


Resolution:
No.  The PID blocks in Unity Pro does not have a setting for ON - OFF control. For ON-OFF control, the output of the PID block can be connected to the input of a PWM function block.