Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can I read a string data from OFS V3.60?

Article available in these languages: Spanish

1) The typical syntax AliasName!%MW returns the numerical value of the string.
image

2) To see the actual data in a string format you need to add the ;c at the end.
AliasName!%MemoryWord;c

M340!%MW10:4;c
image2