Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can we upload programs with Vijeo Designer from the Magelis XBTG/GK/GT, HMIGK/GTO/GTU, HMISTO/STU?

Goals and Symptoms

Can we upload programs with Vijeo Designer from the Magelis XBTG/GK/GT, HMIGK/GTO/GTU, HMISTO/STU?

Causes and Fixes


It is necessary to previously configure the Vijeo-Designer project according to: In the Target's properties, for XBTG/GK/GT, HMIGK/GTO/GTU, HMISTO/STU...
- select download File System
- enable the Include Editor Project in the Download property.
In other words: if the project has not been downloaded with this option, you cannot upload it.