Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to configure the communication between Lexium Controller and OPC?

In the attachment file, you will find a presentation which shows an easy way to configure the communication between Lexium Controller and OPC.
LMC_OPC.zip

This example is based on the freeware:
MatrikonOPC Explorer

You can find it here:
http://www.matrikonopc.com/

Remark: Any other OPC software can be used.


Legacy KB System (APS) Data: RESL192210 V1.0, Originally authored by MaPr on 06/26/2008, Last Edited by MaPr on 06/26/2008
Related ranges: Lexium Controller