Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Lexium32M Profibus: What is the functionality of the "Drive Profile Lexium 2" ?

Goals and Symptoms

Lexium32M Profibus:
What is the functionality of the "Drive Profile Lexium 2" ?

Causes and Fixes

In the attachet ppt file you can find all informations about the "Drive Profile Lexium 2".
A programm example for Siemens Step7 (S7300/400) is available in the M&D TIP database: (Programming Examples -> Lexium32).

Attachments

(Removed File URL: 202810_F1CE/Drive_Profile_Lexium_2.ppt)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/b90b3bd6b2c6dbcec12577520052a065/fl_block_5/0.62E?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL202810 V1.0, Originally authored by StKu on 06/30/2010, Last Edited by StKu on 06/30/2010
Related ranges: Lexium 32

Schneider Electric Saudi Arabia

Attachment(s)
Drive_Profile_Lexium_2.ppt [338.5 KB]