Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
PROGRAM EXAMPLES WITH LEXIUM32

Goals and Symptoms

PROGRAM EXAMPLES WITH LEXIUM32

Causes and Fixes

There are a lot of program examples for Lexium32 with different plc:
Twido, Premium, M340, Magelis HMI, LMC20, LMC058, M238, M258, Siemens, Rockwell, Beckhoff, Mitsubishi, Omron, ....

and different field busses:
CANMotion, CANopen, Modbus TCP, Modbus RTU, Profibus DP, Ethernet IP, Ethercad, pulse/direction.....

Available on M&D TIP database in Lotus Notes

Attachments

(Removed File URL: 203644_025A/Program_examples_with_Lexium32.ppt)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/7bb411f1ff6126f9c12577b40026ab06/fl_block_5/0.642?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL203644 V1.0, Originally authored by PaFr on 10/06/2010, Last Edited by PaFr on 10/06/2010
Related ranges: Lexium 32

Schneider Electric Saudi Arabia

Attachment(s)
Program_examples_with_Lexium32.ppt [533 KB]