Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
with reference to the extension card VW3A58201 and ATS48 - PTC thermistor input, can you please tell me what is the resistance reset value .( 1300 oh...

Goals and Symptoms

with reference to the extension card VW3A58201 and ATS48 - PTC thermistor input, can you please tell me what is the resistance reset value .( 1300 ohms ? )

Facts and Changes

ATV38 - VW3A58201 ATS48

Causes and Fixes

The reset value is 1500 Ohms


Legacy KB System (APS) Data: RESL157681 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altivar 38