Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why does ATS48 need indepent control supply CL1 and CL2 ? On the other hand, how the ATV does not have an indepent control supply as ATV48 has ?

Goals and Symptoms

Why does ATS48 need indepent control supply CL1 & CL2 ? On the other hand, how the ATV does not have an indepent control supply as ATV48 has ?

Causes and Fixes

It's due to the function of the product, the ATV control board is supply by the DC bus and you can program it without start order. For ATS, there is no DC bus but only thyristors command and you need to have a separate suplly for the control.


Legacy KB System (APS) Data: RESL159713 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altistart 48