Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
When trying to attach my Ethernet network to my Ethernet card / port in Unity; why are my networks not showing available in the pull down window?

First the networks must to be created by right clicking on Networks under Communication.


wqerty

From the Unity I/O map double clicking on the Ethernet port will bring up a window asking the user to link a configured network to the card.
efrgt
Often user will try to choose a network and there are no network options available to choose.
frgty


Right click on the particular network from the project tree shown in figure #1 and select Configure; the screen below will open. The Model Family must be chosen for the network. When the mouse is moved over the Model Family list a pop-up window will show the user which Family to choose for which type of network card.
qwerty


Going back into the I/O map and double clicking on the port will now show available networks for that port.