Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does the Advantys STBXMP1100 bus termination plate have to be ordered separately?

Issue:
Does the Advantys bus termination plate STBXMP1100 come with the NIM module or does it have to be ordered separately?

Product Line:
Advantys

Environment:
Advantys Configuration Software

Cause:
Customer not sure if they lost the termination plate and if it comes with it or if it has to be ordered separately.

Resolution:
The Advantys bus termination plate does not have to be ordered separately. The bus termination plate is shipped with each NIM module, however, a replacement bus termination plate can be ordered as part number: STBXMP1100.