Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to optimize the ATV enclosure cabinet dimensions ?

Goals and Symptoms

How to optimize the ATV enclosure cabinet dimensions?

Causes and Fixes

The possibilities to optimize the enclosure dimensions is to increase the air circulation with more air input with filters
Add fans for the cabinet ventilation.
Depending on the customer installation, fresh air can be taken from another side of the cabinet (use filters).
Be careful to not have dusty air inside the cabinet.