Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the differences between the AS-P810-000 and the AS-P810-001 power supplies?

Issue
Suitable replacement for the P810 power supply.

Product line
984 800 series

Environment
P810 power supply

Resolution
Both models of the P810 operate from either a 115VAC or 230VAC power line. The P810-001 includes a power on/off keyswitch and a front accessible fuse. The P810-000 does not offer these two features. With the exception of the keyswitch and the front-mounted fuse, the two power supplies are identical.