Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Converting a ProWORX NxT application that has a Profibus configuration extension defined to a Concept application.

Issue
Converting a ProWORX NxT application that has a Profibus configuration extension defined to a Concept application.

Product Line
Convertion Modsoft - Concept

Environment
Windows 7

Resolution
Use the following procedure to convert a ProWORX NxT application that has "Profibus configured to a Concept project.


1.) Use ProWORX NxT to download the project to the plc.
2.) Use Concept to upload the project from the plc.
3.) Define the number of "Profibus configuration extensions
4.) Add the 140 CRP 811 module to the IO Map.
5.) Click on the 'Parameter' button to bring up the module parameters.
6.) Click on the 'Import' button to import the .cnf file for the Profibus configuration.
3.) Save the application.

Note:

The Profibus related configuration information for the 140 CRP 811 mdoule does not get uploaded from the plc.