Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it possible to run more than one instance of ProWORX NxT at a time on a PC?

Issue

Is it possible to run more than one instance of ProWORX NxT at a time on a PC?

Product Line

ProWORX

Environment

ProWORX NxT

Resolution

No. ProWORX NxT was not designed to have more than one instance of itself open at a time on a PC.