Issue
When configuring the output channels for -10V to +10V on a Momentum 170AMM0900 module in the ProWorx NxT software, what's the difference between the three options Last Value, Full Range and Zero?
Product Line
Modicon Momentum I/O
Environment
170AMM0900
Resolution
-10v to +10v Last Value.....This means that if communication with the CPU is lost, the output channel will retain the last value.
-10v to +10v Full Range.....This means that if communication with the CPU is lost, the output channel will come up at +10v.
-10v to +10v Zero.....This means that if communication with the CPU is lost, the output channel will reset to zero.
Released for: Schneider Electric Saudi Arabia