Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the difference between state flow and power flow?

Issue

What is the difference between state flow and power flow?

Product Line

ProWorx

Environment

ProWorx

Resolution

State flow: An instruction is select if it solves true, regardless of whether instructions "upstream" are passing power. State flow lets you see the state of each contact or coil immediately.
Power flow: An instruction only passes power (is highlighted) if it solves true and the instructions to the left of it also pass power.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre