Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for the programming cable for the TSX07 Nano PLC?

Article available in these languages: Japanese

Issue

What is the part number for the programming cable for the TSX07 Nano PLC?

Product Line

Modicon Nano PLC

Environment

TSXPCX1031

Resolution

The part number for the serial programming cable for the TSX07 Nano PLC is TSXPCX1031. The TSXPCX3030 USB programming cable can alternatively be used but only if the user is using version 4.0 of PL7-07 under WIN2000 Professional.