Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the J890 and J892 RIO drop modules be hot swapped?

Issue
Can the AS-J89x-<example> RIO drop modules be hot swapped?

Product line
Modicon 1/2/3/4/5/984s

Environment
J890

Resolution
No. The J890 and J892 RIO drop modules are not specified for hot swapping. As such, you should power down the drop prior to swapping one out.

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: