Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Load impedance range for STBACO1210 and STBACO1225 Analog Output modules.

Issue

The purpose of this resolution is to inform STB users of the load impedance range for STBACO1210 and STBACO1225 Analog Output modules.

Product Line
Advantys,STB

Resolution

The load impedance may be 0 - 500 Ohms.


Legacy KB System (APS) Data: RESL176388 V1.0, Originally authored by on , Last Edited by on
Related ranges: Advantys STB