Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
140DSI35300 Shunt Resistor Explained

Issue

The purpose of this resolution is to explain why a resistor is added across switching devices connected to a 140DSI35300 Supervised Input Module.
re: Modicon Quantum Automation Series Hardware reference Guide, p/n 840USE10000

Product Line
Quantum

Resolution

If the field connection is good, when the switching device connected to a module input is open circuit, this shunt resistor completes the circuit and provides a small current sensed by the module. This current indicates that field wiring is not interrupted and a complete circuit exists.

The resistor selection is sized so a minimum input current of 0.15 mA is maintained. If input current drops below that, the module will signal a broken field connection in the appropriate bits of I/O mapped Broken Wire registers #3 and #4.