Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Advantys returns 'You do not have sufficient access rights to run this application'

Issue
Advantys Configuration Software .returns 'You do not have sufficient access rights to run this application'

Product Line
All versions of the Advantys Configuration Software.

Environment
Windows 7, Windows 10

Resolution
The Advantys Configuration Software returns the following message when it is started and
the user is logged into the PC as an administrator.

werty

The error is returned because the Advantys Configuration Software cannot find the Temp folder that is
supposed to be in the installed Advantys folder.

To resolve the problem, create a temp folder in the Advantys folder.


Legacy KB System (APS) Data: RESL181419 V1.0, Originally authored by AlCh on 01/04/2007, Last Edited by AlCh on 01/04/2007
Related ranges: Advantys STB