Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Which Magelis XBT-GT HMIs supports an analog camera?

Issue
Which Magelis XBT-GTs supports an analog camera?

Product Line
XBTGT Series HMI (no longer commercialized)

Resolution
There are 4 XBTGT targets that support video:
XBTGT4340
XBTGT5340
XBTGT6340
XBTGT7340.

They all have one analog video input. Therefore, for any of these targets, you can connect one video source.