Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Wiring a 2-wire Transmitter to an STBACI1225 Analog Input

Issue
This resolution describes how to wire 2-wire analog transmitters to the inputs of an STBACI1225 analog input module.


Product Line
Advantys STB
STBACI1225


Environment


Resolution
R2-wire analog transmitters require a loop power supply to power the loop. The following diagram shows how this is done with a single power supply for all current loops.

​​​​​​​