Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the features of the BMXRWSFC032M memory card for the BMXNOE0110?

The BMXRWSFC032M is a 32MB memory and when inserted in the FactoryCast option module BMXNOE0110, it provides services to conform to Transparent Ready class C30. A total of 32MB are available for user web pages and the BMXNOE0110 is delivered with one BMXRWSFC032M already installed.