Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it possible to FTP files out of a M340 PLC with SD card and data storage via the USB port?

Yes you can FTP files out of the M340 PLCs via USB. The USB port is Ethernet like with a IP address of 90.0.0.1.