Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
171CBB97030 Processor/4 Port Switch IEC Exec. Upgrade to v.1.06e

Issue
The purpose of this resolution is to inform 171CBB97030 users that the IEC firmware has been upgraded (August 2008) to version 1.06, for use with Concept 2.6.


Product Line
Momentum
171CBB97030


Environment


Resolution
IEC firmware version 1.06 resolves the following issues:

1) IEC Exec version 1.05 did not allow OFS to access Concept IEC unlocated variables.
2) An xxmit Function Block may fault with an error 150 if the xxmit block is active (powered) while the 171CBB97030 is powered cycled.

Installing IEC firmware v.1.06 (filename: mpsv106e.bin) resolves the above-mentioned issues.