Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to upload editor project from XBT GT / XBT GK / iPC?

Goals and Symptoms

The feature "Upload editor Project" of Vijeo-Designer requires a specific setup in the editor before the download of the application in the HMI target.

Causes and Fixes

The attached document explains:
- how to setup the project in Vijeo-Designer in order to allow the upload of the editor project,
- then how to upload the project from the XBT GT / XBT GK / iPC.

Attachments

(Removed File URL: 192759_6642/How_to_upload_the_editor_project_from_HMI_target.zip)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/8d3da768ddce5831c12574c2005292b2/fl_block_5/0.592?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL192759 V1.0, Originally authored by ArGr on 09/12/2008, Last Edited by ArGr on 09/12/2008
Related ranges: Magelis Compact iPC, Magelis Smart, Magelis XBT GTW, Magelis XBT GK, Magelis XBT GT, Vijeo Designer

Schneider Electric Saudi Arabia

Attachment(s)
How_to_upload_the_editor_project_from_HMI_target.zip [420.08 KB]