Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Do any of the M340 Ethernet modules support the Network Time Protocol (NTP)?

Yes the v2.0 M340 NOEs BMXNOE0100 & BMXNOE0110 do support the Network Time Protocol (NTP).
Note: Unity Pro v4.0 is required for this functionality and it is only available on the M340 NOE modules.