Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the Part Number of the Modicon M340 rack extender module?

Issue

Customer is in search of part number for the M340 rack extender module

Product Line

Modicon M340 PAC

Environment

Hardware/Components

Resolution

M340 Rack extender module Part # BMXXBE1000. This module will only work with Unity Pro 4.0 and higher

See more information here: Modicon M340 PAC | Schneider Electric USA