Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Will the MBX 7.0 drivers work with a Vista 64 bit operating system.

No. At the current time the MBX 7.0 drivers will support only 32-bit Windows Vista/XP/2000/Server 2008/Server 2003.
MBX v7.1 Patch #3 is required for 64 bit PC's.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre