Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can I calculate the heat dissipation on a Magelis XBT-GT5230 from the VA rating on the unit?

Issue
Goal: Example calculation to determine the heat dissipation of a Magelis XBTGT5230 based on the VA rating of the unit.


Product Line
Magelis XBTGT


Resolution
Facts:

  • 1 Watt equals to 3.412 BTU/Hr.
  • Power Factor of the Magelis XBT-GT5230 is almost one. But for heat dissipation calculation we will use 0.8
  • XBTGT5230 Power Consumption: 26VA

To calculate the heat dissipation, you need to consider the type of load you are dealing with. Typically, if you have a capacitive or inductive load, you will need to know the power factor (PF) to convert to Watts:

Watts = VA * PF
VA = Watts/PF
VA = 26/0.8 = 32
.
32 Watts is about 110 BTU/hr.

Therefore, the heat dissipation on a Magelis XBTGT5230 is 110 BTU/hr. Please choose an electrical enclosure accordingly.

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: