Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to configure the STBEHC3020 for event counting

Issue
How to configure the EHC3020 for event counting.

Product Line
All versions of the Advantys Configuration Software.

Environment
Windows 7

Resolution
Wire the 'EHC3020' to the incremental encoder.
c zc
xcz c

  • Double click on the 'EHC3020' module to open the properties window for the module.
zxc c
  • Configure the parameters as shown.
· Download the application to the island.
czx
  • Start the PLC.
· Place the PLC into test mode.
zx  c
  • Set the Input Validation bits to Off.
cxa
  • Set the Counter Enable to On.
ac