Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Configuring Messaging service without checking Access Control box will disable I/O scanning and Global Data services

Issue

To inform users a defect was encountered involving Modbus Messaging (Access Control service) communication.

Product Line

Unity Pro

Environment

Unity Pro v4.0

Resolution

The defect manifests when the Modbus messaging service is not used and access control box under the Messaging tab is not checked but the access control table is configured (there is some lines defined on it). This configuration will disable I/O Scanning and Global Data services.

Customers can resolve this issue in one of two ways:
1) Upgrade to Unity 4.1. It prevents users to fill in any data in the access control table without checking the Access Control box.
2) If using Unity 4.0, do not configure the access control table if you do not plan to restrict module communication. If you want to use the Access Control feature, ensure that you check the Access Control box.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre