Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the level of protection to the mechanical shocks of the XB5S: IK index.

Goals and Symptoms

What is the level of protection to the mechanical shocks of the XB5S: IK index.

Facts and Changes

XB5S
Mechanical shocks
IK

Causes and Fixes

The XB5S is IK03.


Legacy KB System (APS) Data: RESL200556 V1.0, Originally authored by LaBe on 11/23/2009, Last Edited by LaBe on 11/23/2009
Related ranges: Harmony XB5S