Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the system requirements for Concept 2.6 SR6?

1. System requirements for Concept 2.6 SR6:
- x86-based personal computer (Pentium platform recommended)
- Win98, Win2000, or WinNT 4.0 SP3 or higher (Y2K compatibility requires SP5 ), WinXP Pro or Windows Vista Business 32 Bit
- Win95 is no longer qualified. Win3.1x is no longer supported.
- 24 MB application RAM (or higher)
- CD-Rom drive
- 150 MB hard disk space
- VGA graphics adapter and screen (minimum resolution: 800x600)
- Microsoft compatible mouse

Concept 2.6 SR6 does not support Windows 7 Professional (32). You would need to upgrade to Concept 2.6 SR7 to run on Windows 7 (32)

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)