Issue
This Resolution contains the Release Notes for the 140NOE77101 Exec firmware version 6.0.
The attached document describes the Issues, Results, and Customer Actions of the changes to Exec versions 6.0, 5.4, 5.32, 5.3, 5.2, 5.1, 5.0, 4.9, 4.8 and 4.7.
Product Line
Quantum
140NOE77101
Environment
Resolution
Refer to the attached document for the complete details.
NOE77101 Exec v6.0 Release Notes.pdf
NOE77101_v6.0_Release_Notes_20130329.pdf
MBP_MSTR Sub-Function 16 Behavior
MBP_MSTR_Sub-Function_16_Behavior.pdf:
- UPDATE 3/29/13 (doc revision 20130329)
Release Notes for version 6.0 - new excel format - UPDATE 12/21/12 (doc revision 9)
Release Notes for version 5.4 - UPDATE 11/29/12 (doc revision 8)
Release Notes for version 5.32 - UPDATE 9/24/12 (doc revision 7)
Release Notes for version 5.3 - UPDATE 7/13/12 (doc revision 6)
Release Notes for version 5.2 - ICS-ALERT-12-020-03 - UPDATE 7/6/12 (doc revision 5)
added a resolved issue to version 5.1 - UPDATE 6/28/12 (doc revision 4)
Release Notes for version 5.1 - UPDATE 12/15/2011
zip file contains pdf's:
1. Release Notes for version 5.0.
2. Command 15 behavior
3. Sub-Function 16 behavior - UPDATE 7/7/2011
zip file contains pdf's:
1. Release Notes for version 4.9.
2. Command 15 behavior
3. Sub-Function 16 behavior - UPDATE 12/22/10:
1. Release Notes for version 4.8.
2. Added new title to section of Release Notes version 4.7; The NOE is incorrectly assigned an address of 'configured IP+1' instead of the 'configured IP' in a standalone 140CPU6716x.
Released for: Schneider Electric Saudi Arabia