Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the CF cards compatible with Smart iPC and XBTGTW?

Goals and Symptoms

What are the CF cards compatible with Smart iPC and XBTGTW?

Causes and Fixes

The following CF cards are supported:

2GB CF card: MPCYN00CF200N
4GB CF card: MPCYN00CF400N

Note that other CF cards which size is less than 2 GB are not supported by the System Monitor of our Smart iPC and XBTGTW.

512MB CF card: MPCYN00CFE00N
1GB CF card: MPCYN00CF100N

The user is warned with a SMART message of the system Monitor like: Hagiwara sys-com cf-diag error


Legacy KB System (APS) Data: RESL209043 V1.0, Originally authored by MaLy on 09/11/2012, Last Edited by MaLy on 09/11/2012
Related ranges: Magelis XBT GTW, Magelis Smart BOX, Compact PC Box & Flex PC BOX, Magelis Smart