Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How many load cells can be connected to the Momentum Weighing Module 170-ISP-001-00?

Up to eight load cells can be connected to the weighing module. If more than one load cell is used, then the cells must first be connected to a load cell junction box, then to the 15 pin sub D connector on the Momentum base.


Image