Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does the Momentum weighing module require a processor or a communication adapter on top of the base?

No, The weighing module can be run without peer communications or a PLC. The base has it's own on board processor that will hold it's configuration and the values read from the weighing device. A dummy top hat is included with the base to keep out dust and other contaminants from the otherwise exposed components of the base.


Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre