Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is an external 24V loop supply required for current loops with BMXAMI08x0?

Issue
Does the BMXAMI0800 or BMXAMI0810 require an external loop power supply or does the module provide it for the 4-20mA current loops ?

Product line
Modicon X80 IO

Resolution
Yes. Both the BMXAMI0800 and BMXAMI0810 require an external loop power supply for their 4-20mA current loops. The module does not provide it.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre