Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What does a Unity Quantum "Dead error 405 81" indicate?

Dead error 405 is defined as "time out waiting for Modbus Plus"
Sub code 81 means "Prom Checksum error"
During operation the MB+ processor (on the CPU) periodically performs self tests. This error means that the computed checksum was bad.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre