Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Will the latest firmware (v1.44E) for the 140CPU43412A work for a PLC programmed with ProWORX NxT?
Yes. The q5rv144e.bin file supports both Concept (IEC & 984) and ProWORX PLCs.

Schneider Electric Saudi Arabia

Attachment(s)
q5rv144E.bin [400 KB]