Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the maximum distance allowed when using the M340 BMXXBE1000 expansion module.

The Maximum length allowed in the daisy chain of expansion modules is 30 meters.