Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can I read simple ASCII characters into my Quantum PLC via a Network Option Ethernet module (140NOEXXXXX)?

Goals and Symptoms:

Can I read simple ASCII characters into my Quantum PLC via a Network Option Ethernet module (140NOEXXXXX)?

Causes and Fixes:

No. The quantum Network Option Ethernet modules (140NOEXXXXX) can only accept Modbus TCP/IP messaging. They cannot read in ASCII characters. ASCII messaging can be accomplished either via the 140ESI06210 ASCII interface module or via the XMIT (984LL) or XXMIT(IEC) instruction from Modbus port #1 on the CPU module.


Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre