How can we help you today?

How far away from the Circuit Monitor Series 2000 can I mount the RTM (ride-through module)?

Issue:

Customer would like to mount the RTM physically and needs to know the maximum distance allowed from the CM2000 Series.

Product Line:

CM2150

CM2250

CM2350

CM2450

Environment:

Installation of a Ride-Through Module on a CM2000 Series Meter

Cause:

The RTM was installed in a location that did not comply with the required mounting distance from the Circuit Monitor.

Resolution:

The RTM can be mounted on the back of the Circuit Monitor or can be mounted remotely, as long as it is mounted within 10 feet of the Circuit Monitor.

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
  • Product Documentation