Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the screw size and wire sizes for the CT and PT terminal connections on the CM4000 series meters?
Issue
What are the screw size and wire sizes for the CT and PT terminal connections

Product Line
CM4000
CM4250
CM4000T

Environment
Hardware Specifications

Resolution
The terminal screws are 4mm with a 0.7 pitch. Each meter is supplied with spade lugs that accommodate 10-12 AWG wire.